Click here to view this message in a browser window.

Company Contact:

Linda Mecimore
Kollmorgen
540.633.3688

Agent Contact:

Julie Eleftheriou
Longren & Parks
952.913.3065

Please consider the attached news release from Kollmorgen for your upcoming print, online and enewsletter editorial coverage.

Learn How to Reduce Risk of Food Recall and Boost Efficiency Through Hygienic Machine Design with Kollmorgen at IPPE 2016

Visit booth B8016 for live demos of AKMHTM Hygienic Servo motors

RADFORD, VA – December 16, 2015 – Kollmorgen will exhibit its industry-leading motion solutions for food and beverage manufacturers in booth B8016 of the International Production & Processing Expo (IPPE), January 26 – 28, 2016, at the Georgia World Congress Center in Atlanta. Throughout the show Kollmorgen will demonstrate its AKMH Hygienic Servo Motor and enhancements, including the vented connector option, which allows the motor to equalize pressure through the connector assembly. The company is also adding support for the Resolver, Endat Sine Encoder, Hiperface and Optical Encoder feedback devices. 

“The AKMH motor is ideal as a retrofit for legacy and/or competitor servo motors,” said Bill Sutton, Market Development Manager at Kollmorgen. “The AKMH removes the need – and related cost – of replacing an existing drive while delivering increased reliability, durability and cleanability in even the toughest wash-down environments.” 

IPPE attendees are invited to visit booth B8016 to discuss application needs and learn more about how Kollmorgen can help them achieve desired results. Meetings with a Kollmorgen expert can be scheduled by contacting Bill Sutton at Bill.Sutton@Kollmorgen.com.

 

ABOUT KOLLMORGEN

Kollmorgen is a leading provider of motion systems and components for machine builders around the globe, with over 70 years of motion control design and application expertise.Through world-class knowledge in motion, industry-leading quality and deep expertise in linking and integrating standard and custom products, Kollmorgen delivers breakthrough solutions unmatched in performance, reliability, and ease-of-use, giving machine builders an irrefutable marketplace advantage. 

For more information visit www.kollmorgen.com, email support@kollmorgen.com,or call 1-540-633-3545.

AKMH Hygienic Servomotor

AKMH Hygienic Servomotor (click here to download photo)

Copyright © 2015 Kollmorgen 2609

 

Signup for the Kollmorgen eNewsletter

Email preferences can be modified when signing up for eNewsletter above or

click here to unsubscribe.